Gates Europewereldwijd
Europa/Afrika

Europe/Africa: English (EU) français Russkij Deutsch Español Polski Italiano Türkçe Nederlands Ceština

Voor onmiddellijke vrijgave July 15, 2007

Contact: Kathy Brysse

mediaeurope@gates.com

New cooling system catalogue from Gates

Gates releases a new Cooling System Catalogue, providing all required information on cooling system hoses, thermostats and caps for passenger cars and light-duty vehicles in one multilingual catalogue. 
 
The new catalogue has been expanded with 32 additional references in the curved hose range and 36 additional references in the thermostat range. Gates premium quality thermostats provide a precise fit and prevent leakage. Their temperature sensitive heat motor allows precise engine cooling, in order to guarantee optimum engine performance. 
 
An additional feature in Gates’ cooling system catalogue is the completely new range of Unicoil™ hose bending productsThe Unicoil™ consists of a coil, and a bendable spine welded to the coil. By simply positioning the Unicoil™ on the straight hose and by using hand pressure to bend the spine, you can form almost any shaped rubber hose in seconds. The metal spine holds the hose in shape; the stainless steel coil prevents the hose from collapsing or kinking. Unicoil™ is available in seven different diameters, a range that has been carefully selected to provide maximum coverage for the automotive repair specialist.
 
Next to above mentioned novelties the catalogue contains an extensive introduction on Gates products for automotive applications, technical information on Gates cooling system products and a description on how to use the catalogue.  Alphabetical listings by vehicle make identify the matching hose and thermostat references. As usual Gates has also included clearly structured listings to guide the user to the required Gates replacement product for a specific car make, based on the motor type, capacity and model year. A further chapter in the catalogue contains size listings of the Gates cooling system hoses, as well as pictures of all curved hoses and thermostats. With the conversion lists one can easily identify the Gates hose or thermostat corresponding to the OE reference.